AnsweredAssumed Answered

AD9361 RX measures repeatability after reboot

Question asked by lukronos on Feb 22, 2018
Latest reply on Feb 26, 2018 by larsc

Hi,

 

I work with ad9361. I used it in my home made board, in FDD and MGC mode. I use an oscillator for the reference clock signal and I measure the signal from an external source.

 

I use the API from Analog Devices with some little customization in order to work with my application.

 

When I do some measures successively, the RX ports show the same result each time (+/- noises), I can deal with it. The problem is when I restart the ad9361 (by software in calling the ad9361_init function or in hardware in turning on/off), the measures are different than before restrarting (it is not a very big difference, but it is greater than noises).

 

The customable parameters are not modified between before and after restarting.

 

My questions are : what is the cause of this change of measure after calling the ad9361_init function? Do you know how can I solve this?

 

Thanks

 

Regards.

Outcomes