AnsweredAssumed Answered

We are using AD5724/TSSOP24 in one of our project. We have configured the DAC as per the requirements, and able to write and read data from DAC registers. But still we are not getting any outputs in DAC channels, it is showing 0.6V always.  set 10V in DAC

Question asked by maheshk on Feb 21, 2018
Latest reply on Feb 25, 2018 by isantos

We are using AD5724/TSSOP24 in one of our project. We have configured the DAC as per the requirements, and able to write and read data from DAC registers. But still we are not getting any outputs in DAC channels, it is showing 0.6V always.  set 10V in DAC channel A, similar way we tried other channels also.Is sample code availble for AD5724-R  available ?

Outcomes