AnsweredAssumed Answered

AD-FMCDAQ2-EBZ SAM Coaxial connector

Question asked by Mochi on Feb 20, 2018
Latest reply on Feb 22, 2018 by Mochi

I would like to ask you about AD-FMCDAQ2-EBZ.
I hope that this is the right place.


I received the following question from my customer.
What is the characteristic impedance of the ADC input and DAC output of this evaluation board designed with ohms?


As far as I see the circuit diagram, the ADC input and the DAC output are coupled with an RF transformer, and this RF transformer seems to be a 50 ohm product, so the characteristic impedance of the ADC input and the DAC output circuit may be considered 50 ohms Is it?

 

Thank you very much for your attention.


Best regards

Outcomes