AnsweredAssumed Answered

Default AD9361 Rx Bandwith with No-OS SW - 2016_r1

Question asked by beamer.ce1 on Feb 15, 2018
Latest reply on Feb 22, 2018 by DragosB

Hi,

 

Could someone tell me what the default AD9361 Rx bandwidth will be in 1RX1TX mode, using a 40.0 MHz sample rate and running the 2016_r1 release of the No-OS software?

 

Also, is the default Rx BW calculated as a ratio based on the sample rate alone or are there other factors involved in that calculation?

 

Any feedback would be appreciated.

 

- Brad

Outcomes