AnsweredAssumed Answered

(ADV7612)Can ADV7612 support I2S ,Higher than 96kHz, 5.1CH, 24bits?

Question asked by donadona999s on Feb 15, 2018
Latest reply on Feb 15, 2018 by donadona999s

Hi !

 

I have some questions about ADV7612.

 

Q1)

I already understood ADV7612 can not support TDM.

(ADV7612)Can ADV7612 support TDM, I2S ,Higher than 96kHz, 5.1CH, 24bits? 

But  how about if our customer don't use TDM.

Can ADV7612 support 96kHz, 5.1Ch, 24bits?

 

Q2)

At this thread, I already understood ADV7612 can support 8Ch maximum.

(ADV7611)Can ADV7611 sent 7.1ch audio with I2S? 

But I want to make sure what is the highest frequency when our customer use I2S.

For example, ADV7480 can support to 12.288MHz.

(ADV748x)Can ADV748x support TDM, I2S ,Higher than 96kHz, 5.1CH, 24bits? 

=>(8 slots x 32 bits x 48 kHz = 12.288 MHz)

I think ADV7612 will use 32-bits total package size.

So, the maximum frequency should be "2 slots * 32bits * ??kHz = ??MHz"

But I couldn't search I2S port maximum frequency.

Can you tell me the maximum frequency value?

Can ADV7612 handle 96kHz?

 

Best regards

Kawa

Outcomes