AnsweredAssumed Answered

The USB interface of PZSDRCC-BRK-G carrier board doesn't work with the Matlab firmware

Question asked by EtanV on Feb 15, 2018
Latest reply on Feb 15, 2018 by travisfcollins

Hello All,

 

I'm struggling with starting the USB connectivity of PicoZed SDR2 PZSDRCC-BRK-G carrier board with combination with the Matlab firmware, which supports Communications System Toolbox™ Support Package for Xilinx® Zynq®-Based Radio, but without any success till this moment.

USB works perfectly with the Analog Device's zynq-picozed-sdr2-brk firmware but not with the Matlab's one.

When I insert USB pen drive there is no any indication for connectivity. Nothing from fdisk -l, lsusb and into the /dev/bus/ directory.

Has anyone encountered the same issue before?

 

Thank you so much for any idea how to overcome that issue.

 

Regards,

 

Ethan

Outcomes