AnsweredAssumed Answered

External EEprom in LTC 2984 module

Question asked by tshivam on Feb 15, 2018
Latest reply on Feb 23, 2018 by LoganC

I am using LTC 2984 demo board (DC 2399 A) for temperature measurement. I am designing a  PCB using LTC 2984 LQFP for other custom sensor applications. My question is that is it possible to use the internal EEPROM of 2984 without the external EEPROM as given in DC 2399A   and in DC 2210A daughter board.
If there is an internal EEPROM in LTC 2984, then what is the use of External EEPROMs in DC 2399A and DC 2210A daughter board.

Thanks,

Shivam

Outcomes