AnsweredAssumed Answered

RSSI slot

Question asked by s.kannan on Feb 14, 2018
Latest reply on Feb 26, 2018 by sripad

I had a doubt regarding slot used in RSSI measurement. What is the slot that was mentioned in the RSSI measurement topic (pg 53 in UG-570)?

Is it same as the gain update counter interval?

It is also mentioned that there are 4 measurement values(if Default meas. bit is clear), whose sum will give Total RSSI measurement duration. My doubt is that all these 4 measurement are done during the single RSSI calc slot or each measurements are done in each separate RSSI calc slot?

Outcomes