AnsweredAssumed Answered

LT5560LT5560 component :0.01MHz to 4GHz Low Power Active Mixer

Question asked by siddharthgoyal on Feb 12, 2018
Latest reply on Apr 4, 2018 by wsapia

For my application the signal output port(Pin 5&6) frequency range is from 1KHz to 20KHz, so according to Table7 & Figure 3 its working for 10MHz with L3=L4=0 i.e. no external component is required, only transformer is required for impedance matching.  So, "will this configuration work for 1KHz-20KHz (much lower frequency) output"  No information is available for such lower frequency IF output in the datasheet.

Outcomes