AnsweredAssumed Answered

Multichannel select in TDM mode for adsp-21584

Question asked by MZC on Feb 9, 2018
Latest reply on Feb 20, 2018 by Jithul_Janardhanan

Hi,

What are the maximum number of channels select in TDM mode?

 

There are total 16 individually configurable HSPORT(0A-7A and 0B-7B) in ADSP-21584, each HSPORT can select 128 channels. It means that total 128*16 = 2048 channels are selectable. Is it correct?

 

On the hardware manual, on page 34-33, it is written that

"In multichannel mode, the SPORT can selectively transfer data on up to a maximum window size of 128 continuous
channels out of a maximum 1024-channel frame while ignoring all the disabled channels within the window
and all the channels outside the window. "

 

Why selectable channels are limited to 1024? Is there any limitation to select channels (apart from clocking)?

 

Best Regards,

 

Mussab Zubair

Outcomes