AnsweredAssumed Answered

Linux Kernel Driver support for ADIS16465

Question asked by krisklau on Feb 8, 2018
Latest reply on Feb 8, 2018 by NevadaMark

Hi,

 

I am looking for Linux driver support for the newly released ADIS16465. It is my understanding that the interface should be similar to the earlier IMU's in the 164xx series, so the AD kernel driver (ADIS16480 IIO Inertial Measurement Unit Linux Driver [Analog Devices Wiki] ) should only need minor changes.

 

1. Is there plans for official support for this device?

2. If I want to adapt it myselves, which of the earlier devices matches closest to 16465 in terms of register access method and triggering?

 

Best regards,

Kristian

Outcomes