AnsweredAssumed Answered

ADV7611 Vertical Frequency Change!

Question asked by Qammar on Feb 8, 2018
Latest reply on Feb 9, 2018 by Qammar

Hi,

I have a 1024x768 @60Hz video as input to the ADV7611. However, i need resolution of 1024x768 @50Hz at the output but there is no option for 1024x768 @50Hz in the HDMI Graphics Mode. However, there is an option of V_FREQ[2:0] in ADV7611, that is used in free run mode. If i set it to 50Hz, and somehow enter the free run mode will i get an output video with vertical frequency 50Hz? Thank you!

Outcomes