AnsweredAssumed Answered

ADV7511- Scrip required

Question asked by FreddyS on Feb 6, 2018
Latest reply on Feb 15, 2018 by GuenterL

Hello

Can we get a working script for the ADV7511 with the default values for all the registers and the setting of the relevant registers we need to configure for the below setting:

The input video (BT656):

 

  • D0 – D7: BT656 8 bit interlace YCbCr 4:2:2     720x480/30 or 720x576/25
  • CLK – Clk from BT generator

 

OUTPUT (HDMI):

  • HDMI to monitor: 480i/576i and 480p/60 or 576p/50 ; we need the configuration register to set the output in each option
  • DVI: Where to control the scaling from 720x480 to 640x480 VGA

Thanks

Freddy

Outcomes