AnsweredAssumed Answered

ADV8005 Sample code Rx input setting

Question asked by Fermat on Feb 4, 2018
Latest reply on Feb 7, 2018 by Poornima

Hi,

 

I am check ADV8005 Evaluation board with Rx(7625) input, but it cannot output.

I use command, but there is still no output.

 

Does "BF_7625_8005_VSP_1.91.RC1_20160526.zip" support Rx? I check other source from ADV7842, it's OK.

Can teach me how to set command to output?

 

BTW, i check the sample code of ADV8005, it seems there are RxInitTable setting for RX input in "8005_top_hal.c".

But these code are comment out.

Should I make these code compiler if I want to use RX?

 

 

Thanks

Ken

Outcomes