AnsweredAssumed Answered

ADF5355 Init Problem

Question asked by tooony on Feb 1, 2018

Hello,

 

i try to control a microwave using the ADF5355 from the microcontroller ATmega328P. The microwave generator is a custom board running with 38,4 MHz reference frequency. With the ADF5355 we want to generate signal withe frequency range from 9,5 GHz...10,5 GHz (10 GHz for normal). The ADF5355 Board is a custom board developed from an extern company. I got the information that the setup runs with a 38,4 MHz reference clock and that i should use an PFD of 76,8 MHz.

 

My code on the microcontroller generates the register entries. I validated the generated resgisterentries and the look like the same as in the Evaluation Board Control Software. So far so good - But i cant get the ADF5355 working and i get no lock.

 

At first i try to geht the init sequence to work. Here i have (analog to the datasheet) to use the init sequence, which init first with the halved PFD ( init for pfd > 75 MHz). Here is my first question: Is the halved PFD the half of the PFD in normal operation or the the half of the reference clock?

 

Can you explain more about the workflow to init the ADF5355? Here are my register entries for the halved PFD part of the init sequence (from register 12 to 0):

 

0x0001041C
0x0061300B
0x00C0183A
0x1000C419
0x102D0428
0x120000E7
0x35002406
0x00800025
0x30009F84
0x00000003
0x00040032
0x03555551
0x00200820

 

After init with halved pfd i expected to get a lock, but i dont get a lock. When i run the complete init sequence for pfd > 75 MHz i get a other frequency then 10 GHz. I use the digital lock, so i expect that the muxout pin goes to a stable high level (3,3 volt) - is that right?

 

I hope for some help to geht the ADF5355 working. In addition is the screenshot of the configuration for the wanted setup in normal operation (10 GHz with PFD 76,8 MHz).

Outcomes