AnsweredAssumed Answered

I'm interfacing to an A/D input from an unbalanced lumped element RF chain using a transformer (MABA-007159-000000).  The transformer has amplitude imbalance of 1 dB and phase imbalance of 7 degrees.  I'm modeling the imbalances using ADS at the A/D input

Question asked by david2018 on Jan 30, 2018
Latest reply on Jan 30, 2018 by DougI

Allocation of Amplitude & Phase Imbalances at A/D input

Outcomes