AnsweredAssumed Answered

ADRF6720-27

Question asked by masoudmr on Jan 30, 2018
Latest reply on Apr 4, 2018 by THA

I have a problem with the output power of ADRF6720-27, It's output power is about -16dbm while in datasheet said it is about 0dBm. i read and checked all registers and input power of baseband inputs and i think they are OK. Can anyone help me to improve the output power? Should i enable anything else?

Thanks.

ref input: 50MHz

PFD: 25 MHz

Output Freq: 2550MHz

BaseBand : 10MHz, 1 Vp-p

Outcomes