AnsweredAssumed Answered

PicozedSdr-BRK reference design for IIO Oscilloscope

Question asked by keisn13 on Jan 29, 2018
Latest reply on Apr 30, 2018 by mhennerich

Hello, I have picozed sdr with brk board. Using quick start guide i replaced BOOT.bin file on flash, and this works fine with IIO Oscilloscope. 

If I create new BOOT.bin file from source on flash (bit+fsbl+uboot) this also works fine with IIO Oscilloscope.

After this i tryied to create project from ADI git repository (hdl/projects/pzsdr2/ccbrk_lvds at master · analogdevicesinc/hdl · GitHub ). Project was compiled fine, but:

1) size of bit file is lower then on flash: 13M vs 4M

2) IIO Oscilloscope doesn't work. It crashing after click "Refresh".

As i understood, that project in ADI git is not the same as on flash. Could you  please help to find reference design for picozed sdr 2x2 brk, which will produce the same bit-file as on a flash and will works fine with IIO Oscilloscope.

--

Best regards, Michael.

Outcomes