AnsweredAssumed Answered

HMC557A as an Upconverter

Question asked by Moti_Y on Jan 26, 2018
Latest reply on Jan 29, 2018 by huangzeyan

Hello all,

In the HMC557A data sheets there is a spurious performance table for the standard down conversion case.

Can you please provide a similar table but for the up conversion case (i.e. input is the IF port, Output is the RF port).

Any up conversion table will help me but I am interested specifically in the following frequency ranges:

Lo: approx. 4 GHz.

IF input: 120 to 600 MHz

RF output: 4.1 - 4.6 GHz

 

Thank you for the prompt response

Outcomes