AnsweredAssumed Answered

ADI Linux (xemacps) driver for 1000 Mbps speed of ethernet1 on Picozed SDR

Question asked by abhinav004 on Jan 26, 2018
Latest reply on Jan 29, 2018 by abhinav004

Hi,

I have an issue bringing up 1Gbps speed of ethernet1 on custom board which is modeled on Picozed SDR. It is able to work with 10/100 Mbps speed, but gives frame errors in case of 1000 Mbps. However, 1000 Mbps works well with Picozed SDR with default ADI Linux SD card image.

I know this is not a good place to ask about this issue, but just wanted to know if there were any special modifications done for Picozed SDR in xemacps driver(to support1000 Mbps speed & gmii2rgmii module) available with the ADI Linux SD card image? I don't have the liberty to switch to the latest MACB driver for ethernet1.

I am using the xcomm_zynq branch of ADI kernel source for my project.

 

Regards,

Abhinav

Outcomes