AnsweredAssumed Answered

ADF5355 lock time / timeout values for low PFD frequencies

Question asked by cp4an on Jan 25, 2018

I use the ADF5355 with an PFD frequency of 1.024 MHz:ADF5355 register settings

I measured lock time that is much longer than 3.5 ms. I like to lower the lock time so I changed Timeout values and measured minimum and maximum lock times:

tlock_min [ms]tlock_max [ms]alcslvctl
2,283,65222
3,14,610422
3,54,915622
3,425,3820822
4,227,04301222

To me it sees that ALC Timeout of 30 is only useful for high PFD frequencies like 61MHz.

I use following equations:

alc = 30                                = 30                                             [ADF5355 Datasheet rev.d, p.35]

sl = alc / 2,5                          = 30/2,5 = 12                              [ADF5355 Datasheet rev.d, p.35]

vc = ceiling(fpfd /2400000)   = ceiling(1024/2040)            = 1  [ADF5355 Datasheet rev.d, p.35]

tl = ceiling(fpfd * 50µs/alc)    = ceiling(1024000*50µs/30) = 2 [ADF5355 Datasheet rev.d, p.35]

 

To me it seems that ALC is to much for a PFD frequency like 1.024 MHz.

How can I compute ALC Timeout for my application to lower lock time with reliable lock detect?

You will find attached the ADF4355 Software config file for the ADF5355 Software.

Attachments

Outcomes