AnsweredAssumed Answered

HMC960 additional parameters

Question asked by kirill.koval@eltech.spb.ru on Jan 23, 2018
Latest reply on Jan 23, 2018 by jdobler

Hello. 

Are following parameters measurements (that are absent in datasheet) can be open ?

There are about:

1) OIP3(over frequency fI_IF=0-100 MHz):
• HMC960 has Zin=400 Ohm @input impedance = 400 Ohm, output impedance = 100 Ohm (Standard Bias Setting mode);
• HMC960 has Zin=100 Ohm @input impedance = 100 Ohm, output impedance = 100 Ohm (Standard Bias Setting mode);
• HMC960 has Zin=400 Ohm @input impedance = 400 Ohm, output impedance = 100 Ohm (Hight Linearity Bias Setting mode);
• HMC960 has Zin=100 Ohm @input impedance = 100 Ohm, output impedance = 100 Ohm (Hight Linearity Bias Setting mode);

2) Noise Figure of HMC960 for the following conditions:
• NF (f_IF=0-100 MHz) in case HMC960 has Zin=400 Ohm @input impedance = 400 Ohm, output impedance = 100 Ohm;
• NF (f_IF=0-100 MHz) in case HMC960 has Zin=100 Ohm @input impedance = 100 Ohm, output impedance = 100 Ohm.

 

Thanks!

Outcomes