AnsweredAssumed Answered

Ethernet on blackfin 536

Question asked by saif.ub on Jan 23, 2018
Latest reply on Feb 20, 2018 by VineethaThomas

Im using adsp536 dsp processor ,i need to do ethernet protocol on it.

I'm using dp83848i ethernet PHY through MII interface.

well i see that there is lwip stack support on on visual dsp++ update 7.

 

lwip stack is ported to vdk kernel.

 

when i make use of lwip application project in vdsp++ ,it is straight  entering in to  idle condition.

 

is it because ADI ethernet driver doesn't support 536, or

 have any changes to be made??

 

can u tell me the initialization procedure or any demo for this.

 

looking forward to your reply.

Outcomes