AnsweredAssumed Answered

Generating at least two tones with AD9910

Question asked by ahm@ on Nov 23, 2011
Latest reply on Dec 1, 2011 by ahm@

Hi All,

 

I am trying to get two sinusoidal signals at the output of AD9910 demo board. I have used RAM modulation mode but in RAM mode loaded data is being switched with address step rate as usual. I need to have 100MHz and 101MHz output (Also 1MHz-100MHz output). How can I get these signals with evaluation board software or should I program externally?

 

Best Regards

Outcomes