AnsweredAssumed Answered

Flash write without JTAG

Question asked by Andrew.Choi on Jan 22, 2018
Latest reply on Feb 2, 2018 by Jithul_Janardhanan

One of my customers is looking for a way to write to Serial Flash via UART communication without using JTAG.

Is there a method that can write to Serial Flash with UART communication?

Please let me know if there is a method or a technical document which can write to Serial Flash by UART communication.

 

Flatform

DSP : BF523 / Tool VDSP++ 5.1.2 or CCES 2.7.0 (Now uses VDSP++)

 

In addition, ADZS-USB-ICE only supports up to Windows 7 in the technical documentation. Can I use it for Windows 8 or later?

 

Thank you

Outcomes