AnsweredAssumed Answered

AD9371 custom profile

Question asked by kristen123 on Jan 22, 2018
Latest reply on Feb 16, 2018 by gverma

Hello everyone,I develop AD9371 in my custom board.I create custom profile with AD9371 Filter wizard v1.10, I  load custom file into AD9371 Transceiver Evaluation Software to get c script,  However I found my code will return error when execute RX DC Offset Calibration,the initErrCode is 3 which means Calibration time out--loop back receiver(LBRx),I have totally  no idea why this is happen.Besides,When i use the standard profile which is provided by AD9371 Transceiver Evaluation Software.It will not return the error.I don't konw if there is something wrong with the custom profile.

Here is my custom profile.

Another question is if I choose TX_OFF,Do I still need to set the TX RF_PLL?

And why can't choose ObsRX  OFF in the AD9371 Transceiver Evaluation Software?Do the ObsRX must open?

Outcomes