AnsweredAssumed Answered

关于AD9364的时钟输入和AD9517的谐波抑制问题?

Question asked by zhus116 on Jan 21, 2018
Latest reply on Jan 22, 2018 by lallison

1、请问AD9364的参考时钟输入是否可以输入差分时钟,分别连接它的P和N脚可以吗。我看了AD9364的开发板,他用的是无源晶振两个管腿的20MHz的输入,我是否可以采用AD9517的out4的LVDS的时钟输出20MHz直接作为AD9364的参考时钟输入?

2、AD9517的一次二次输出谐波非常大,二次达到了-10dBc左右,有什么办法可以配置它的本身抑制它输出的谐波吗?

3、AD9364的时钟输入有什么其他要求,例如输入的参考时钟的一次、二次谐波需要抑制到多少,如果它的输入一次谐波-45dBc,二次谐波有-30dBc左右可以吗,它的输入时钟必须是正弦波吗,削顶的正弦波或者方波可以吗?

Outcomes