AnsweredAssumed Answered

Can the AD8513 be powered by a single 5 V supply?

Question asked by lmirkin on Jan 20, 2018
Latest reply on Jan 23, 2018 by lmirkin

Hello,

 

I have been using the AD8513 opamp, powered by a single 5 V power supply, as a buffer at the output of a DAC and have noticed that the input offset voltage is rather high: I've seen it as high as 20 mV. The datasheet doesn't explicitly say that the device cannot be powered by a single supply, but I'm now wondering if that isn't the case.

 

Could someone please confirm?

 

Thanks in advance,

Leo

Outcomes