AnsweredAssumed Answered

Migrating ADAU1452 to ADAU1466

Question asked by PSU-4 on Jan 18, 2018
Latest reply on Feb 1, 2018 by DaveThib

Hello,

 

I would like to replace ADAU1452 with ADAU1466 in an existing project. Hardware seems to be no problem (I built a prototype with ADAU1466 and it works with the old software) since these two are pin compatible. That's great!

 

Is there an easy way to exchange ADAU1452 with ADAU1466 in SigmaStudio? When I try to delete ADAU1452 from the config I get the message "The selected IC is being used by one or more algorithms ..." which is understandable. But I'm wondering if there is a way to migrate my design to the new 1466 without completly re-drawing everything.

 

Any helpful tips or ideas are greatly welcome.

 

Thank you!
Bernd

Outcomes