AnsweredAssumed Answered

ADM2484E Vdd2

Question asked by HOD on Jan 17, 2018
Latest reply on Jan 18, 2018 by RAnslow

Hi

 

I have a question ADM2484E.

 

ADM2484E DS is write,

'The logic side of the device can be powered with either a 5 V or a 3.3 V supply, whereas the bus side requires an isolated 3.3 V supply.'

 

And ,

Vdd2 ABSOLUTE MAXIMUM RATINGS is 6V max.

 

Vdd2 can use 5V supply?

 

Best Regards

HOD

 

Outcomes