AnsweredAssumed Answered

What is the effect on ADG508A about a floating input?

Question asked by sguirand on Jan 16, 2018
Latest reply on Jan 31, 2018 by EricC

Hi,

 

I'm working with two ADG508AKR connected to an ADC (AD7880CR) through an OP297GS.

On one of the multiplexer, I have an input which is an option to my design. When this option is not installed, the input is floating.

We are reading each channels (except the floating one) in a loop. In this loop, we are selecting the channel, then proceeding to the ADC conversion, then reading the ADC Data.

We observed some glitch when reading the ADC data around the floating input.

 

Is a floating input can cause an issue on the MUX selection?

Is there any recommendation about unused input? 

 

Thanks,

Sabine G.

Outcomes