AnsweredAssumed Answered

ADL5373 Output frequency range

Question asked by AkiraO on Jan 17, 2018
Latest reply on Feb 22, 2018 by AkiraO

Hello,

 

I'd like to confirm the output frequency range of ADL5373. According to the datasheet, the output frequency range is 2300MHz to 3000MHz. And the modulation bandwidth is >500MHz. Does the output frequency range include the bandwidth? (It can support 2550MHz to 2750MHz for the carrier, in case of 500MHz bandwidth.) Or is 2300MHz to 3000MHz for the career frequency?

 

Best regards,

Akira

Outcomes