AnsweredAssumed Answered

AD9364 initialization error

Question asked by WojciechPIT-PL on Jan 15, 2018
Latest reply on Feb 13, 2018 by DragosB
Hello,

I am trying to install drivers for AD9364 from this page:

https://github.com/analogdevicesinc/no-OS/tree/master/ad9361

I copy files from the "sw" and "platform_xilinx" folders to the "sw / src" folder, in the project in the Xilinx SDK according to the following instructions:

https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/baremetal?doc=AD9364_Reference_Manual_UG-673.pdf

For this project I am exporting hardware from the pzsdr1_ccbrk_lvds file. Then I created the FSBL project in the SDK for this hardware, and then to empty project  which i created, I'm copying the drivers. Then I create using the "create boot image" tool, the BOOT file containing the .elf files - from the FSBL application and the sw.elf file from the sw / Debug folder and the system_top.bit file from the system_top_hw_platform folder.
I put the created Boot file in the SD card. I place the card on the ADRV9364 board embedded in the ADRV1CRR-BOB board. I connect the USB cable to the UART-USB interface. At the terminal i see the error.
error
Please help
 

Outcomes