AnsweredAssumed Answered

ADP5054 Absolute Maximum Ratings

Question asked by sss on Jan 15, 2018
Latest reply on Jan 17, 2018 by JustinZhao

Hi all,

 

Absolute Maximum Ratings in the datasheet @ ADP5054 is following,

SWx to PGND : −0.3 V to +18 V

Is it input or output spec. ?

 

The output voltage ripple our customer observed is about -3V.
Like the Figure 6 @ UG-816 ADP5054-EVALZ User Guide .

Is it over voltage or not, −0.3 V > -3V ?


Best regards,

sss

Outcomes