AnsweredAssumed Answered

ADV7619 questions

Question asked by S.O. Employee on Jan 11, 2018
Latest reply on Jan 18, 2018 by XavE

Our customer is having questions for ADV7619. They have some monitors that can use RXA_5V. And some of the monitors they are using can not use RXA_5V. However, they have to use both monitors when HDMI cable connect to the monitors. Therefore, they propose the following methods.

 

[1] Monitor CABLE_DET_A_RAW and switch between DIS_CABLE_DET_RST0 or 1.

   (a)CABLE_DET_A_RAW =1(Detect 5V

   ⇒use DIS_CABLE_DET_RST0

   (b)CABLE_DET_A_RAW =0Not detect 5V

   ⇒use DIS_CABLE_DET_RST1

 

[2]   Set DIS_CABLE_DET_RST1 all the time when they use RXA_5V and don't use RXA_5V.

Is it possible that this method as above [1] or [2] run ADV7619 correctly?

Also, Could you tell us anything if [1] and [2] methods can't be used?

 

Please comments.

 

Outcomes