AnsweredAssumed Answered

Indication of Calibration completion

Question asked by s.kannan on Jan 10, 2018
Latest reply on Jan 11, 2018 by mhennerich

while moving back to Rx state in TDD mode, I write 0xFF to register 0x016, indicating commencement of all calibration through the command:

echo 0x16 0xFF > direct_reg_access

But after few seconds, while I tried to read the register again(0x16 reg. will self clear the bit when the corresponding calibration are finished), its showing 0x3F ( which indicates Tx quad. cal. , RF DC Cal., BB DC cal are still running)

I also write 00 to register 0x35 and 0xFF to 0x36. While I monitor the control pin D7 (cal done), its showing 1 which indicates all the calibrations are done but 0x16 reg is reading 3F which indicates few calibrations are running.

What does this mean?

Which one I should believe?

Outcomes