AnsweredAssumed Answered

Configuring problem in AD5755-1

Question asked by pruthvikumar019 on Jan 9, 2018
Latest reply on May 7, 2018 by rrosario

I have followed the sequence mentioned in flowchart given in datasheet to configure AD5755-1.  I have configured control register and trying to read back same register but, I did not get any data on SOUT. Please send us the initializing sequence for the following requirements: I need to supply a 10mA current in all the 4 Channels. I have AD0=1 and AD1=0, External resistors of 15K at RSET pin. External capacitor of 10nF at COMPDCDC pins. I have CLEAR pin LOW and LDAC pin HIGH.

Outcomes