AnsweredAssumed Answered

Multiple measurements AFE loop or sequence?

Question asked by CDiego on Jan 5, 2018
Latest reply on Jan 9, 2018 by mark.ramos

Hi,

 

 I'd to take multiple 4 wire measurements without changing the channels, so far the solutions that I could come up were these:

 

1. Create a for loop to run adi_AFE_RunSequence multiple times. Indicating to which part of a data storage array it should write in each iteration.

 

2. Create a sequence in which once I get the first measurement, I enable the ADC conversion, wait 13ms, disable it, and then enable it and so on... until I get all the measurements.

 

I think the first one would be a slow solution since it would be constantly calling the adi_AFE_RunSequence function. While the second would require multiple lines of the same code, and say for example that I need to take 1000 measurements the code would be a mess and I'm assuming the size of the FIFO would not allow me to get that far.

 

Is there a workaround for this type of problem? should I create a custom adi_AFE_RunSequence?

 

Kind regards,

Diego

Outcomes