AnsweredAssumed Answered

How to set up AD9172 in mode 12 (12-bit High Density)

Question asked by dcurry13 on Jan 5, 2018
Latest reply on Mar 20, 2018 by landsman

I am using an ADS7-V2EBZ and DPG Downloader to provide 12-bit patterns. I also have a test setup using the ZCU102 Zynq Ultrascale+. In both cases, the JESD link is up and running and I can see data being transmitted via Xilinx ILA debugger, but I detect no signal on either TX0 or TX1 outputs besides a spike at the sampling frequency.

 

Is there any documentation on this?? I have verified the functionality of multiple 16-bit modes but cannot get a 12-bit mode to work, not even using exclusively AD dev. boards and tools. The datasheet says nothing of 12-bit mode configuration save for JESD link parameters, which I have ensured are correct.

 

Please advise!!

 

-Dan

Outcomes