AnsweredAssumed Answered

ADL5906  - Output Voltage without the Input Signal

Question asked by nagarajud on Jan 5, 2018
Latest reply on Jan 5, 2018 by andy_m

Hello,

 

We used the below shown schematic with ADL5906, in our existing developed board

Our operating frequency is 2700MHz to 3100MHz and need to detect the signal levels ranging from 0dBm to -55dBm.

But, we are getting an output voltage of 0.9 to 1.1V without the input signal to device and with the external supply feeding. The same level is observed even when we do 50OHM termination at C189 (18pF, as shown in schematic)

 

With this issue we are not able to detect our signals < -45dBm.

 

Please help us to proceed further

Outcomes