AnsweredAssumed Answered

cf_axi_adc not appearing in dmesg

Question asked by daniel_cain on Jan 3, 2018
Latest reply on Jan 5, 2018 by daniel_cain

Thank you in advance for any help and/or clarification. This is really confusing me.

 

I'm working on a development project using the AD9643-250-EBZ board with the FMC interposer and the Xilinx ZC706 carrier board. I am currently trying to build a zynq boot image using an ADI hdl project modified to use the AD9643. Currnetly, I am booting the ZC706 using the image and device tree files from the zynq-zc706-adv7511-ad9265-fmc-125ebz folder. The GUI boots correctly.

 

My question is: I have checked the dmesg output, expecting to see a line containing the string "cf_axi_adc", but it doesn't appear. Is this normal, or is something wrong?

 

I have tried it with the interposer plugged and unplugged from the FMC LPC connector, but it shouldn't matter because I expected to see at least an error message. I also checked the output of lsmod and no driver modules are loaded. Is this normal too, or a problem?

Attachments

Outcomes