AnsweredAssumed Answered

Issues running IIO Scope using ADRV9364 and ADRV1CRR-BOB

Question asked by SirJanA on Jan 3, 2018
Latest reply on Jan 21, 2018 by SirJanA

I am using the ADRV9364 with the ADRV1CRR-BOB.  Using the latest SD card image I was able to get IIO-Scope running.  However, I cannot get it to consistently operate smoothly.  When I set the ip address using ifconfig on the ADRV9364 in linux, every few seconds or so it resets and disappears, and I have to keep doing setting up the ip address.  What ends up happening is the IIO-Scope loses connectivity and therefore I am unable to use IIO Scope effectively.  I can see the samples coming in for a few seconds and then it stops.  Is there an issue with the ADRV1CRR-BOB or the Linux image?  I have tried the IIO-Scope in both Windows and in Linux.  I also have 2 ADRV9364 and 2 ADRV1CRR-BOB and the issues are on both.

Outcomes