AnsweredAssumed Answered

How to boot zc706 from sd card default image

Question asked by kharobangdo on Jan 3, 2018
Latest reply on Jan 3, 2018 by CsomI

I am using zc706 board & FMCOMMS5 board. I am following the procedure given in this ADI webpage. I downloaded the zynq image & copied it on the sd card. Copied the BOOT.bin from the required directory & inserted the sd card into zc706 & powered on the board. The uart terminal shows boot up status & has booted up. Now in the above link I have gotten stuck at BOOT section specifically the one where Uboot default environment needs to be changed 

When I typed the command "env default -a" into the uart terminal it says no such file or directory

Where do I enter this command. How should I proceed.

Outcomes