AnsweredAssumed Answered

Can scripts or CLI be used to control VisualAnalog / ADS7?

Question asked by voot on Jan 2, 2018
Latest reply on Jan 30, 2018 by UmeshJ

I would like to test the AD9208-3000EBZ together with the ADS7-V2EBZ over temperature cycles.

 

I did want to set this up as an automated test rather than using VisualAnalog and having to click the run button for each test.

 

Is there a script / command line interface to visual analog to enable more automated tests? Or, can ADS7 be driven directly to arm and retrieve data?

 

thanks for relevant answers

Outcomes