AnsweredAssumed Answered

SigmaStudio Using Wrong Safeload Address

Question asked by AlthafIsmail on Dec 21, 2017
Latest reply on Jan 2, 2018 by AlthafIsmail

I'm working with ADAU1450 and SigmaStudio v3.15.3 Rev1741 connected via USBi interface on SPI.  I noticed that whenever I change an EQ block, SigmaStudio uses "Safeload Write" operation to push the command to the DSP.  The thing is, it uses 0x6024 as the safeload address while the compiler output says 0x6000 should be the correct one.

 

Capture window:

 

Compiler log:

 

*_PARAM.h:

 

Am I doing something wrong or is this a bug?  And is there a workaround for this?

Outcomes