AnsweredAssumed Answered

About AD7366 Input Range

Question asked by Yuya on Dec 21, 2017
Latest reply on Dec 25, 2017 by Yuya

Hi,

My customer is trying to use the AD7366.
So I got a question.

 

#1 As a customer, he seems to want to input 0 to 12 V as an input range.

  In this case, should I set Vdd = + 12 V, Vss = -12 V, reference voltage = 3 V and RANGE 1, 0 both 1?

   

  If I want to select input ranges other than ± 10 V, ± 5 V, 0 V to 10 V, do I select "Do not program" in Table

  8 in the data sheet?
       Is there a proper use of the setting of ± 12 V and 0 V to 12 V?

 

Best Regards,

Yuya

Outcomes