AnsweredAssumed Answered

AD-FMcomms 5 Sync signal setting

Question asked by maekawa on Dec 20, 2017
Latest reply on Jan 3, 2018 by travisfcollins

We are receiving radio waves using Ad - fmcomms 5 and ZC 702.
In addition, the control application uses 'iio oscilloscope'.

In order to perform 4ch synchronous reception, set the frequencies of Rx and Tx to the same value and set the sync signal as 'FPGA setting'
I know that it is necessary to set frequency and power, but is it there?

In that case, the frequency must be set within the Nyquist frequency for the sampling frequency to be set,
When trying to receive a signal of a band exceeding the sampling frequency, it interferes with the synchronization signal,
It seems that it is not possible to synchronize well, but how is it?

Outcomes