AnsweredAssumed Answered

flash programming problem

Question asked by dasco16321632 on Nov 17, 2011
Latest reply on Jan 27, 2015 by CraigG

Hello,

i have this piece of code....

it builds fine with only two warnings :

 

"C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\214xx\include\cs_macros.h", line 611: cc0047: {D} warning:

          incompatible redefinition of macro "ADSP_2146x_DDR2_Enter_PD"

          (declared at line 401)

  #define ADSP_2146x_DDR2_Enter_PD()\

          ^

 

"C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\214xx\include\cs_macros.h", line 615: cc0047: {D} warning:

          incompatible redefinition of macro "ADSP_2146x_DDR2_Exit_PD"

          (declared at line 405)

  #define ADSP_2146x_DDR2_Exit_PD()\

 

 

when i tried to program the flash i get this error:

 

 

Error: There was a problem with one or more
required expressions in the driver.  Please make
sure the following expressions are present and
try again:
"AFP_BreakReady"
Error: Driver load failed.

 

What is the problem??

any help is more than welcome

Outcomes