AnsweredAssumed Answered

CCES 2.7.0 debug target fails to connect

Question asked by Magicbean on Dec 13, 2017
Latest reply on Dec 21, 2017 by Kader.M

I had been using CCES 2.3.0 and had a project connected to the BF706M eval board. I have both debugged the board on the target using the Debug Agent and programmed the flash so that the board can boot standalone.

 

I have had to reinstall Windows and my development machine is up and running, I have been evaluating various RTOS kernels and now I find I am unable to connect to the target board.

 

The Windows Device Manager shows that the driver is installed

The driver version reported is 4.0.0

 

But when I try to debug any project (including the one which was originally working) I get an error:

 

and in the console I get:

 

Trying to debug also causes the driver to apparently unload itself and the Crosscore Tools entry in the Device manager disappears until I disconnect the BF706 EZ-kit and reconnect it.

Any ideas what is causing this? 

 

Thanks.

Outcomes