AnsweredAssumed Answered

(ADuM14x)How to calculate the supply current when each channel's duty and frequency are not same.

Question asked by donadona999s on Dec 7, 2017
Latest reply on Dec 15, 2017 by donadona999s

Hi !

 

I already asked about the supply current about ADuM14x.

(ADuM140E1)Supply current. 

I want to make sure about it.

At the past thread, it is possible to calculate the supply current if all channel's frequency and duty are same.

But if our customer use this device with not same frequency and duty for each channel, the can not calculate the supply current.

So my questions are these.

 

Q1)

To calculate the supply current, I made new formula.

ADuM140
IDD1 = IDD1(Q) + (2.8mA * D_A + 0.01mA/Mbps * F_A)

                           + (2.8mA * D_B + 0.01mA/Mbps * F_B)

                           + (2.8mA * D_C + 0.01mA/Mbps * F_C)

                           + (2.8mA * D_D + 0.01mA/Mbps * F_D)
IDD2 = IDD2(Q) + (0.02mA/Mbps * F_A)

                           + (0.02mA/Mbps * F_B)

                           + (0.02mA/Mbps * F_C)

                           + (0.02mA/Mbps * F_D)

 

ADuM141
IDD1 = IDD1(Q) + (2.8mA * D_A + 0.01mA/Mbps * F_A)

                           + (2.8mA * D_B + 0.01mA/Mbps * F_B)

                           + (2.8mA * D_C + 0.01mA/Mbps * F_C)

                           + (0.02mA/Mbps * F_D)
IDD2 = IDD2(Q) + (0.02mA/Mbps * F_A)

                           + (0.02mA/Mbps * F_B)

                           + (0.02mA/Mbps * F_C)

                           + (3.4mA * D_D + 0.01mA/Mbps * F_D)

 

ADuM142
IDD1 = IDD1(Q) + (2.8mA * D_A + 0.01mA/Mbps * F_A)

                           + (2.8mA * D_B + 0.01mA/Mbps * F_B)

                           + (0.02mA/Mbps * F_C)

                           + (0.02mA/Mbps * F_D)
IDD2 = IDD2(Q) + (0.02mA/Mbps * F_A)

                           + (0.02mA/Mbps * F_B)

                           + (3.4mA * D_D + 0.01mA/Mbps * F_C)

                           + (3.4mA * D_D + 0.01mA/Mbps * F_D)

* D_A = Duty for A channel input
* F_A = Frequency for A channel input
* D_B = Duty for B channel input
* F_B = Frequency for B channel input
* D_C = Duty for C channel input
* F_C = Frequency for C channel input
* D_D = Duty for D channel input
* F_D = Frequency for D channel input

Are these formula correct?

 

Q2)

If these formula correct, I want ask one more thing.

I think our customer can calculate typical value with this.

But cannot calculate the maximum value because there are no maximum specification for these value.

Is it very difficult to calculate the maximum value?

I think ADI do the production test for 0-50-100% only so I think it is very difficult to calculate the maximum value.

 

Best regards

Kawa

Outcomes